Standard package - up to 5 peopleComfort Package - up to 6 peoplePremium package - up to 12 persons
I confirm that I have read the information that the personal administrator is Mitsubishi Electric Europe B.V. sp. z o.o. Branch in Poland. The data will be processed in order to respond to the inquiry submitted using the above form. The processing of data for these purposes is a legitimate interest of the controller (Article 6(1)(f) RODO). More information about the principles of data processing, including rights (among others, the possibility of filing an objection) is available at link.
I would like to receive messages from Mitsubishi Electric Europe B.V. Sp. z o.o. Branch in Poland/Polish Branch, based in Balice at ul. Krakowska 48, 32-083 Balice, about promotional offers, product information, special actions and events organised by Mitsubishi Electric using the email address I have provided.