News Releases
FOR IMMEDIATE RELEASE No. 3280
TOKYO, May 7, 2019 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the launch of three new Large DIPIPM+™ transfer-mold intelligent power modules featuring loading-converter circuits that realize simpler and more compact designs for use in air-conditioner and industrial inverters. Of special note, one of the new modules achieves a world's first* high-density output of 100A/1200V in its transfer-mold package. Sales of the new DIPIPM+ series will begin on May 29. Also, the modules will be exhibited at major trade shows, including Power Conversion Intelligent Motion (PCIM) Europe 2019 in Nuremberg, Germany from May 7 to 9 and PCIM-Asia 2019 in Shanghai, China from June 26 to 28.
Mitsubishi Electric has been contributing to the miniaturization and energy-efficiency of inverter systems since commercializing its first DIPIPM™ series in 1997. The more compact and simpler-design DIPIPM+ series, which places the inverter and converter into one package, was introduced in 2015. In response to increasing demands for high-power compressors in package air conditioners, the company is now adding models of up to 100A/1200V for package (heat & cooling) air conditioners in the 56kW class.
New Large DIPIPM+ series
| Product | Model | Specification | Release date |
|---|---|---|---|
| Large DIPIPM+ series | PSS50NE1CT | 50A / 1200V | May 29, 2019 |
| PSS75NE1CT | 75A / 1200V | ||
| PSS100NE1CT | 100A / 1200V |
Note that the press releases are accurate at the time of publication but may be subject to change without notice.